Trane Rental Services has an impressive array of HVAC, power
generation and compressed air equipment. We can provide a single unit
or a combination of units and build a solution to fit your needs. Our
capabilities include 1-1,000-ton units of cooling, 36-1,500 kW of
power generation, electric and indirect fired heaters up to 512,000
Btus, and 800 to 1,500 cfm Oil-Free Air units.
Education
Schools and colleges have many unique temporary HVAC and power
needs. Repairs and upgrades cannot always be scheduled during times
when classes are out of session, but Trane Rental Services can keep
classrooms unaffected during scheduled maintenance. Trane Rental
Services can keep students and faculty focused on schoolwork rather
than the temperature of the building. School administrators can rent
chillers or other temporary cooling components to be installed quickly
and easily to keep systems running while repairs or up- grades are made.
Healthcare
Trane Rental Services provides an array of healthcare building
temporary power and cooling solutions. Power and HVAC systems are
crucial for the health of patients. If heating or cooling systems fail
or if they need to be shut down temporarily, the results could be disastrous.
Many healthcare facility managers put a contingency plan into place
as part of their emergency preparedness program. Trane’s rental
emergency equipment often factors into these plans to help healthcare
building HVAC administrators sustain patients’ comfort in the event of
a catastrophe.
Industrial
Manufacturing and chemical operations often have unique industrial
HVAC needs that Trane temporary rental chillers can help solve.
Manufacturers and laboratories sometimes need a temporary cooling
system to back up critical manufacturing and chemical processes. In
many cases, these businesses do not have redundancy or backup systems
in place to minimize downtime. Usually these highly critical and
sensitive processes could cause serious problems for the businesses or
labs if the industrial HVAC system fails; so Trane’s temporary
solutions are the perfect fit.
Trane offers standby equipment programs to provide peace of mind and
minimize financial risks associated with downtime. Trane also has
equipment that can be used during planned shut-down events or in
during the seasons that require supplemental equipment.