Trane Expands its Sintesis Advantage™ Air-Cooled Portfolio with New High-Efficiency CXAF Heat Pumps

The new Sintesis™ Advantage heat pumps fulfil seasonal demands for cooling and heating with versatile configuration options that can increase efficiency up to 20 percent.

Brussels, Dec. 13, 2018 – Trane®, a leading global provider of indoor comfort solutions and services and a brand of Ingersoll Rand, introduces CXAF, a new line of high efficiency large air-cooled heat pumps within its Sintesis™ Advantage portfolio. The new units can fulfil both cooling and heating demands of medium to large sized commercial buildings delivering best in class efficiency levels.

“With the development of the CXAF we aim to make the air-cooled heat pump technology more affordable and advance the electrification of heating to offset the use of fossil fuels for heating and thus reduce our carbon footprint,” said Jose La Loggia, vice president and general manager of Trane in Europe. “This new heat pump aligns with innovation strategy to offer our customers more options for sustainability and better efficiency without sacrificing quality or reliability.”

The new Sintesis Advantage CXAF air-cooled heat pumps are now available across Europe in capacities ranging from 280 to 700 kilowatts (kW) offering wider operating map versus the legacy products. The CXAF can operate down to negative 15 degrees Celsius producing hot water of 40-45 degrees Celsius without the need for auxiliary heating, making it suitable for most European climates and a more reliable and efficient alternative for gas or fuel boilers.

Compact, modular design based on the Sintesis platform and reversible technology allows the unit to operate as a chiller during the summer period. This reduces the volume of equipment needed in a building and lowers installation, maintenance and total lifecycle costs.

The Sintesis Advantage CXAF offers customers more configuration options compared to the legacy product. Customers can now choose between fan technologies and sound packages in order to make the right choice between cost, efficiency and sound level and tailor the system to their specific application.

The units offer best in class, Eurovent Class A efficiency in heating and seasonal efficiency exceeding minimum regulatory requirements. The CXAF HEat (High Efficiency) version features an advanced suction line gas heat exchanger that boosts heating capacity with virtually no impact on energy consumption, increasing efficiencies in both full load and part load up to 20 percent compared to legacy products.

All units in the Trane Sintesis Advantage portfolio are compliant with all applicable European Ecodesign Regulations under the Energy-related Products (ErP) framework Directive 2009/125/EC of the European Parliament.

For more details of on the complete Trane Sintesis portfolio of chillers and heat pumps, please visit Trane.eu.

# # #

About Ingersoll Rand

Ingersoll Rand (NYSE:IR) is a world leader in creating and sustaining safe, comfortable and efficient environments in commercial, residential and industrial markets. Our people and our family of brands — including Club Car®, Ingersoll Rand®, Thermo King® and Trane® — work together to enhance the quality and comfort of air in homes and buildings, transport and protect food and perishables, secure homes and commercial properties, and increase industrial productivity and efficiency. Trane solutions optimize indoor environments with a broad portfolio of energy efficient heating, ventilating and air conditioning systems, building and contracting services, parts support and advanced control. Ingersoll Rand is a $14 billion global business committed to sustainable business practices within our company and for our customers. For more information, visit www.ingersollrand.com or www.trane.com.

Contact Information

Geraldine Velner

Communications Leader, Trane Technologies EMEA

+32493282676

geraldine.velner@tranetechnologies.com

Michal Karkoszka

Contractor, Trane Technologies

+48222435357