Avoiding heat stress for healthcare
The public hospital was challenged to provide enough cooling in the different wards during the hot summer season.
Learn MoreWith quick 24/7 availability, our reliable fleet of Rental chillers, rooftops and heat pumps is the best option when a fast recovery of cooling or heating is required.
Trane Rental Services feature a wide-ranging fleet of chillers, heat pumps and rooftops from 10 kW to 2 MW, able to fulfil any need.
A rental unit is the ideal back-up for a broken or low-performing unit, without any long-term commitment. No need to rush on an expensive repair or replacement – a rental unit can buy you time and peace of mind while delivering the cooling or heating you need.
A chiller is designed to cool down a liquid such as water or brine. The heat removed from the fluid can be dissipated on an integrated condenser or remotely through a cooling tower or dry cooler.
A rooftop is a packaged unit that directly cools the air. Ideal for air conditioning or dehumidification thanks to quick connections through flexible or rigid air ducts. All it needs is an electricity supply, the rest is there.
Compared to other rental companies, at Trane we are committed to decarbonising heating in order to help our customers reduce their CO2 footprint. Our core heating product offering is 100% electric and much more efficient than any traditional heater. On top of that, they do not burn any fuel and have zero local emissions.
A heat pump uses either renewable or waste energy sources to efficiently and reliably deliver warm or hot water for many uses (domestic hot water, process water, heating water). The water-to-water version can also be used to provide cooling and heating at the same time, for unprecedented efficiency.
A rooftop is a packaged unit that directly heats the air. Ideal for space heating thanks to quick connections with flexible or rigid air ducts. All it needs is an electricity supply, the rest is there.
Tell us what you need
The public hospital was challenged to provide enough cooling in the different wards during the hot summer season.
Learn MoreThis modern manufacturing facility in the north of The Netherlands continually invests in innovation and industry-leading technology.
Learn MoreA winery in the Murfatlar vineyard region of Romania needed temporary cooling during the vintage season.
Learn MoreMulti-platinum artist Ariana Grande came to Europe in 2019 with the Sweetener World Tour.
Learn More