Contact your Trane Rental Expert

EaaSy Sharing

Sharing is caring for our planet

For every customer with a seasonal demand for cooling or heating there is always another customer with an opposite need. Natural resources are limited, so sharing the same equipment halves the impact on the planet.

Partnering for the next level in sustainability

Trane Rental Services are the centre point between two customers who can share the same piece of equipment, fully utilised across the year, without the need to build a second machine.

  • Cut consumption of natural resources by 50%

    Cut consumption of natural resources by 50%

    When two or more customers share the same piece of equipment, we eliminate the need to build an extra unit, thus reducing the consumption of copper, aluminium, steel and energy. Wasting is a choice, not a need.

  • As good as owning your own equipment

    As good as owning your own equipment

    Trane Rental Services will deal with all logistics, commissioning and maintenance aspects to deliver the same – or better – service level compared to a traditional ownership model. If you notice a difference, it will only be positive. You need cooling or heating, not a chiller or a heater.

  • Trane reliability, efficiency and service coverage

    Trane reliability, efficiency and service coverage

    All our rental equipment is perfectly maintained according to the highest standards. Our customers can count on our extensive network of service engineers for outstanding 24/7 support. It’s all included.

A valid concept for many customers and applications

Air conditioning is typically a summer business, with chillers and rooftops working hard to ensure comfort during the hottest season. In wintertime, owning a chiller is just inconvenient: it requires “winterization” to avoid frost damage, as well as maintenance for statutory (F-Gas) compliance as a minimum. You can eliminate the inconvenience by sharing the chiller with Trane Rental Services. We call it EaaSy.

Ideal for seasonal cooling or heating applications

Ice rinks – cooling in wintertime

Ice rinks – cooling in wintertime

Ice rinks –typically operating between December and March – are the most obvious example of a seasonal need for cooling. The rental option means they can share a chiller with the many summertime cooling applications.

Wineries – extra cooling in summertime

Wineries – extra cooling in summertime

Depending on the local climate, wineries might have a constant demand for cooling in their wine stores. During summer, when the wine-making process starts, there is a spike in cooling demand which can be perfectly managed with a shared chiller.

Commercial buildings and shopping centres – extra cooling in summertime

Commercial buildings and shopping centres – extra cooling in summertime

Commercial buildings and shopping centres see cooling demand peak in summertime as a result of warmer outdoor temperatures. Extremely hot days have become the norm in recent times.

Resources

Customer Stories

Related Solution